How to port uboot and linux in T4160

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to port uboot and linux in T4160

ソリューションへジャンプ
1,475件の閲覧回数
radhika
Contributor II

Hi ,

We are using powerpc T4160 in our board and need to port uboot and linux with kernel version above 3.0 .I am new in this and would like to know how to get the uboot and the linux for this.

Could anyone please help with this?

Thanks and Regards,

Radhika

1 解決策
1,309件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP offers Linux SDK 1.9 for the T4240 boars. This SDK provides Linux kernel 3.12.37.

NXP offers Linux SDK 2.0 for the T4240 boars. This SDK provides Linux kernel 4.1.30.

See the following page:

https://www.nxp.com/support/developer-resources/run-time-software/linux-software-and-development-too...

 

See the Section 3.3.2 of NXP SDK 2.0-1703 documentation about kernel customizing:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 

See also AN4814 about porting U-Boot and Linux to T4240 Systems:

https://www.nxp.com/docs/en/application-note/AN4814.pdf?fsrch=1&sr=3&pageNum=1


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,310件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP offers Linux SDK 1.9 for the T4240 boars. This SDK provides Linux kernel 3.12.37.

NXP offers Linux SDK 2.0 for the T4240 boars. This SDK provides Linux kernel 4.1.30.

See the following page:

https://www.nxp.com/support/developer-resources/run-time-software/linux-software-and-development-too...

 

See the Section 3.3.2 of NXP SDK 2.0-1703 documentation about kernel customizing:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 

See also AN4814 about porting U-Boot and Linux to T4240 Systems:

https://www.nxp.com/docs/en/application-note/AN4814.pdf?fsrch=1&sr=3&pageNum=1


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,309件の閲覧回数
radhika
Contributor II

Thank you so much for the details.

Regards,

Radhika

0 件の賞賛
返信