How to load RCW in flash on T2080RDB via TRACE 32?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to load RCW in flash on T2080RDB via TRACE 32?

385 次查看
ChristinaK
Contributor II

Hi,

We are trying to load our custom RCW generated from CODE WARRIOR- QCVS tool, onto the T2080RDB.  We are flashing our RCW at 0xf8000000 via TRACE 32. But it is taking default RCW values on the board. 

Can you provide us the correct address and method of loading custom RCW so that our processor reads our custom RCW values?

Any help would be appreciated.

Regards,

Christina

标签 (1)
0 项奖励
回复
1 回复

337 次查看
yipingwang
NXP TechSupport
NXP TechSupport

NXP doesn't support TRACE 32.

You could use CodeWarrior to do flash programming.

Please refer to the following link.

https://community.nxp.com/t5/CodeWarrior-Development-Tools/Flash-Programmer-for-CodeWarrior-Power-Ar...

 

You need to program RCW at address 0xe8000000.

0 项奖励
回复