How to erase/write nor flash using T1042 IFC ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to erase/write nor flash using T1042 IFC ?

2,337 Views
anilakcelik
Contributor I

Hi;

I try to erase and write operation with t1042 integrated flash controller, but  Nor flash is 128 MB and also sector size is 128 KB, sector count 1024.

Erase/write start address is 0xe8fe0000 and sector ending address 0x8ffffff.  

First of all, I run u-boot , then I read random nor flash address with a volatile unsigned integer pointer.  Although I set registers ifc_cspr0_WP (chip select property register, write protect) read/write accesses is allow, i don't write or erase related nor address. I check common event and error status register (ifc_cm_evter_stat) and nor event and error status register, it seems normally, they don't indicate error.

But I don't understand this ifc norcr (nor control register) and nor flash control machine. Moreover, what is the number of phase in ifc_norcr. Why use this total number of phases ? 

Related nor flash datasheet is spansion S29GL01GS. Mentioned datasheet ; address and data on which register to write. Otherwise erase state command transition issue handled with ifc on instead of me.

For example; Commend sequence; Sector Erase; Cycles 6; Addr 555; Data AA.

How to directly erase and write nor flash using ifc? Please detailed me, or show me. 

Thank u.

Labels (1)
0 Kudos
Reply
3 Replies

2,205 Views
ufedor
NXP Employee
NXP Employee

The erase/write procedure of the NOR Flash is not a simple task and there is no such example code.

In U-boot you could refer to the "drivers/mtd/cfi_flash.c".

2,205 Views
anilakcelik
Contributor I

Thank u, but I also read related device datasheet, amd cfi commands etc. (related problem resolved with unlock cyclec command etc).

There is one basic question; is  IFC bus driver necessary ? or all set related IFC registers are enough ?

I read all related nor flash register and also IFC registers thanks to u-boot.  

Firstly i started with u-boot then i run related nor flash code with u-boot, but now i only want to run  IFC driver code + nor flash code with my bootloader.  

0 Kudos
Reply

2,205 Views
ufedor
NXP Employee
NXP Employee

Sorry, as I wrote there is no simple example of the IFC NOR Flash programming.

0 Kudos
Reply