Hi,
I got the following error when trying to add the packages.Please suggest the solution
WARNING: Host distribution "Ubuntu-16.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |#######################################################################################################| ETA: 00:00:00
Loaded 3202 entries from dependency cache.
NOTE: Error during finalise of /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/sources/poky/meta/recipes-connectivity/openssh/openssh_7.6p1.bb
ERROR: ExpansionError during parsing /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/sources/poky/meta/recipes-connectivity/openssh/openssh_7.6p1.bb: Failure expanding variable do_install: ExpansionError: Failure expanding variable do_install, expression was autotools_do_install
if [ "${@bb.utils.filter('DISTRO_FEATURES', 'pam', d)}" ]; then
install -D -m 0644 /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/sshd /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/etc/pam.d/sshd
sed -i -e 's:#UsePAM no:UsePAM yes:' /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/etc/ssh/sshd_config
fi
if [ "${@bb.utils.filter('DISTRO_FEATURES', 'x11', d)}" ]; then
sed -i -e 's:#X11Forwarding no:X11Forwarding yes:' /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/etc/ssh/sshd_config
fi
install -d /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/etc/init.d
install -m 0755 /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/init /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/etc/init.d/sshd
rm -f /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/usr/bin/slogin /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/usr/share/Ssh.bin
rmdir /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/var/run/sshd /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/var/run /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/var
install -d /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image//etc/default/volatiles
install -m 644 /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/volatiles.99_sshd /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image//etc/default/volatiles/99_sshd
install -m 0755 /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/openssh-7.6p1/contrib/ssh-copy-id /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/usr/bin
# Create config files for read-only rootfs
install -d /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/etc/ssh
install -m 644 /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/etc/ssh/sshd_config /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/etc/ssh/sshd_config_readonly
sed -i '/HostKey/d' /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/etc/ssh/sshd_config_readonly
echo "HostKey /var/run/ssh/ssh_host_rsa_key" >> /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/etc/ssh/sshd_config_readonly
echo "HostKey /var/run/ssh/ssh_host_dsa_key" >> /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/etc/ssh/sshd_config_readonly
echo "HostKey /var/run/ssh/ssh_host_ecdsa_key" >> /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/etc/ssh/sshd_config_readonly
echo "HostKey /var/run/ssh/ssh_host_ed25519_key" >> /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/etc/ssh/sshd_config_readonly
install -d /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/lib/systemd/system
install -c -m 0644 /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/sshd.socket /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/lib/systemd/system
install -c -m 0644 /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/sshd@.service /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/lib/systemd/system
install -c -m 0644 /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/sshdgenkeys.service /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/lib/systemd/system
sed -i -e 's,@BASE_BINDIR@,/bin,g' \
-e 's,@SBINDIR@,/usr/sbin,g' \
-e 's,@BINDIR@,/usr/bin,g' \
-e 's,@LIBEXECDIR@,/usr/lib64/openssh/openssh,g' \
/home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/lib/systemd/system/sshd.socket /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/lib/systemd/system/*.service
sed -i -e 's,@LIBEXECDIR@,/usr/lib64/openssh/openssh,g' \
/home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/etc/init.d/sshd
install -D -m 0755 /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/sshd_check_keys /home/suchita/GCR/v2/QorIQ-SDK-V2.0-20160527-yocto/build_t1040d4rdb-64b/tmp/work/ppc64e5500-fsl-linux/openssh/7.6p1-r0/image/usr/lib64/openssh/openssh/sshd_check_keys
which triggered exception AttributeError: 'module' object has no attribute 'filter'
Summary: There was 1 WARNING message shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.