Hello.
I am confused how to display the IFC frequency on the T1020 board.(Blue letter below)
CPU0: T1020, Version: 1.1, (0x85210011)
Core: e5500, Version: 2.1, (0x80241021)
Single Source Clock Configuration
Clock Configuration:
CPU0:1200 MHz, CPU1:1200 MHz,
CCB:600 MHz,
DDR:800 MHz (1600 MT/s data rate) (Asynchronous), IFC:300 MHz
........
SDK1.7 and SDK2.0 display methods are different. Which one is more correct?
1) SDK 1.7 uboot
#if defined(CONFIG_FSL_IFC)
ccr = in_be32(&ifc_regs->ifc_ccr);
ccr = ((ccr & IFC_CCR_CLK_DIV_MASK) >> IFC_CCR_CLK_DIV_SHIFT) + 1;
sys_info->freq_localbus = sys_info->freq_systembus / ccr;
#endif
2) SDK 2.0 uboot
sys_info->freq_localbus = sys_info->freq_systembus / CONFIG_SYS_FSL_IFC_CLK_DIV;
Best regard.
已解决! 转到解答。
#if defined(CONFIG_FSL_IFC)
ccr = ifc_in32(&ifc_regs.gregs->ifc_ccr);
ccr = ((ccr & IFC_CCR_CLK_DIV_MASK) >> IFC_CCR_CLK_DIV_SHIFT) + 1;
sys_info->freq_localbus = sys_info->freq_systembus / ccr;
#endif
According to the code above, IFC clock freq in uboot means the external clock freq of IFC, not the IFC IP module clock freq. In fact IFC external clock isn’t used on any existing board, so the right way is to calculate IFC IP module clock freq in uboot log as below:
sys_info->freq_localbus = sys_info->freq_systembus / 2.
SDK 2.0 is correct.
#if defined(CONFIG_FSL_IFC)
ccr = ifc_in32(&ifc_regs.gregs->ifc_ccr);
ccr = ((ccr & IFC_CCR_CLK_DIV_MASK) >> IFC_CCR_CLK_DIV_SHIFT) + 1;
sys_info->freq_localbus = sys_info->freq_systembus / ccr;
#endif
According to the code above, IFC clock freq in uboot means the external clock freq of IFC, not the IFC IP module clock freq. In fact IFC external clock isn’t used on any existing board, so the right way is to calculate IFC IP module clock freq in uboot log as below:
sys_info->freq_localbus = sys_info->freq_systembus / 2.
SDK 2.0 is correct.