How to change the map memory(PCI and T2080)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to change the map memory(PCI and T2080)

跳至解决方案
1,847 次查看
manoloruiz
Contributor III

Hi,

I would like to change the memory map for PCI devices in T2080RDB. I have tried changing the dtb. However, I get a kernel error when I try to access memory position. I guess it is fixed in the CCSR register but I would like to know how to do it.

I would like to know:

-How to change any value in the CCSR register.

-Which register I should change in order to change the map memory for a PCI.

Thanks!

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,551 次查看
Pavel
NXP Employee
NXP Employee

Look at attached file. It is u-boot configuration file for the T2080RDB board from SDK 1.9. Look at PCI bus configuration in this file.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,552 次查看
Pavel
NXP Employee
NXP Employee

Look at attached file. It is u-boot configuration file for the T2080RDB board from SDK 1.9. Look at PCI bus configuration in this file.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复