FMAN µCode for T2081

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FMAN µCode for T2081

Jump to solution
893 Views
ralftruebenbach
Contributor III

Hello,

which fman µcode do I have to use for the T2081? Is "QorIQ Linux SDK v2.0 PPC64E6500 IMAGE.iso/t2080qds-64b/fsl_fman_ucode_t2080_r1.1_108_4_5.bin" from QorIQ Linux SDK correct?

Kind regards,

Ralf

Labels (1)
Tags (3)
0 Kudos
1 Solution
552 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

The T2080 and T2081 has the same FMAN, so customer can use the ucode for both devices. There are two T2080 microcodes – _106_ and _108_. You can look for its features in

http://git.freescale.com/git/cgit.cgi/ppc/sdk/fm-ucode.git/tree/readme?id=fsl-sdk-v2.0
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
553 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

The T2080 and T2081 has the same FMAN, so customer can use the ucode for both devices. There are two T2080 microcodes – _106_ and _108_. You can look for its features in

http://git.freescale.com/git/cgit.cgi/ppc/sdk/fm-ucode.git/tree/readme?id=fsl-sdk-v2.0

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos