Hi All,
I am working Ethernet on T4160RDB-64B. I want to configure the Ethernet MUX Configuration. The default RCW value for RGMII and I configured to GPIO.
I want to configure the following Ethernet Pins,
EC1_TX_EN/GPIO3_12
EC1_TXD3/GPIO3_08
EC1_TXD2/GPIO3_09
EC1_TXD1/GPIO3_10
EC1_TXD0/GPIO3_11
EC1_RX_DV/GPIO3_14
EC1_RX_CLK/GPIO3_15
EC1_RXD3/GPIO3_16
EC1_RXD2/GPIO3_17
EC1_RXD1/GPIO3_18
EC1_RXD0/GPIO3_19
EC1_GTX_CLK125
EC1_GTX_CLK/GPIO3_13
Regards,
VinothS
Solved! Go to Solution.
To configure EC1 pins as GPIO3 it is required to set RCW[EC1]=10 - refer to the QorIQ T4240 Reference Manual, Table 4-13. RCW Field Descriptions, EC1.
The EC1_GTX_CLK125 does not have secondary function - refer to the QorIQ T4160/T4080 Data Sheet, Table 1. Pinout list by bus, Ethernet Controller 1.
To configure EC1 pins as GPIO3 it is required to set RCW[EC1]=10 - refer to the QorIQ T4240 Reference Manual, Table 4-13. RCW Field Descriptions, EC1.
The EC1_GTX_CLK125 does not have secondary function - refer to the QorIQ T4160/T4080 Data Sheet, Table 1. Pinout list by bus, Ethernet Controller 1.
Hi Uferdor,
Thank you for reply. So, if I configured as GPIO in RCW no needs to done any pin configuration and it will take automatically secondary function
Is it right?
Regards, VinothS
Yes.
Thank you ufedor