During SD RCW Boot SD DAT0 stuck Low

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

During SD RCW Boot SD DAT0 stuck Low

559 Views
kylevonschmacht
Contributor I

To whom it may concern,

We're working on binging up a T2081 based board, derived from the T1042RDB and T2080RDB.  cfg_rcw_src pins are set for SD card boot. 

Observing the Pins shows an active clock, and command sequences sent on CMD, however DAT0 is constantly held low. DAT[1:3] are all held high.

The same SD card when used in the T2080RDB shows activity on DAT0, other pins read the same our board.

What might be going on?

Thanks for your help,

Kyle

Labels (2)
0 Kudos
1 Reply

412 Views
Pavel
NXP Employee
NXP Employee

Test the SDHC DAT0 pin behavior using u-boot booting from different source. For example, test your board using u-boot from NOR Flash.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos