Dmesg ouput of T4240RDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dmesg ouput of T4240RDB

409 Views
sareenakp
Contributor II

Hi,

I am new to kernel programming. I would like to redirect the kernel dmesg output via the UART2 of T4240RDB.

What is the procedure for the same?

I found the links which which describes the generic process Electronics FAQ: Redirecting kernel messages (dmesg) out through your serial port

But on T4240RDB ttyS0 (UART1) is used for the console to access the linux from the host.

Now , I want the dmesg output to be redirected to the ttyS1 (UART2) of T4240RDB.

Is it possible . What are the steps to achieve it. Should I add a boot parameter in the u-boot?

A quick response is appreciated as I am stuck with an issue here.

Thanks in advance.

Sareena.

Labels (1)
Tags (3)
0 Kudos
0 Replies