DPAA Qman and Bman private memory set-up

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DPAA Qman and Bman private memory set-up

跳至解决方案
1,599 次查看
PaulWalker
Contributor III

The T1040RM says the DPAA Bman and Qman need to be allocated some private memory. I'm doing this upon Core0 start-up; as the manual says this only needs to be done once. However, does the private memory require valid context on each core, i.e. a TLB entry on each core? My operating mode is AMP with a Memac MAC available on each core.

Thanks

0 项奖励
回复
1 解答
1,576 次查看
yipingwang
NXP TechSupport
NXP TechSupport

There is only one private area needed for QMan regardless of if it is AMP or SMP, the memory is used exclusively by QMan so it doesn't matter how many cores they are using. Same with BMan. This private area is used by the QMAN and BMAN, not used by CPU cores.

TLB is for entire SoC, it is not setup per core OR per AMP.

Customer may refers to the SDK2.0 User Guide for high level concept on partitioning and virtualization.
e.g.
https://docs.nxp.com/bundle/GUID-39A0A446-70E5-4ED7-A580-E7508B61A5F1/page/GUID-90B41092-EE2D-4741-B...
https://docs.nxp.com/bundle/GUID-39A0A446-70E5-4ED7-A580-E7508B61A5F1/page/GUID-9FA2A089-F316-4063-A...

在原帖中查看解决方案

3 回复数
1,577 次查看
yipingwang
NXP TechSupport
NXP TechSupport

There is only one private area needed for QMan regardless of if it is AMP or SMP, the memory is used exclusively by QMan so it doesn't matter how many cores they are using. Same with BMan. This private area is used by the QMAN and BMAN, not used by CPU cores.

TLB is for entire SoC, it is not setup per core OR per AMP.

Customer may refers to the SDK2.0 User Guide for high level concept on partitioning and virtualization.
e.g.
https://docs.nxp.com/bundle/GUID-39A0A446-70E5-4ED7-A580-E7508B61A5F1/page/GUID-90B41092-EE2D-4741-B...
https://docs.nxp.com/bundle/GUID-39A0A446-70E5-4ED7-A580-E7508B61A5F1/page/GUID-9FA2A089-F316-4063-A...

1,561 次查看
PaulWalker
Contributor III

Hi,

Thanks for the info. That's great.

You said "TLB is for entire SoC, it is not setup per core OR per AMP."

This is not my understanding. My understanding is that LAW, IFC, etc. are part of the SoC so have global context and are set-up once. TLB is a feature of the E500-series core L2MMU, so has core context. As such, TLB is set-up per-core so that each core can have a different context.

0 项奖励
回复
1,551 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Sorry about the confusion. I do mean LAW, not TLB. My apology for typo.

0 项奖励
回复