DDR controller DQ mapping register - how to interpret the TRM section 14.4.49

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR controller DQ mapping register - how to interpret the TRM section 14.4.49

360 Views
trevorfox
Contributor III

Hi,

I have a custom board that I have received four of. It has a T1042 with attached DDR3L memory, 72 bit data bus.

Three of the four boards has functional DDR, the fourth is intermittent failures when SW loads the DDR. I am trying to use the NXP Codewarrior QCVS DDR validation tool but it is failing initialization, and I recall from another project that due to the data bits being swizzled on some of the byte lanes, the DQ mapping registers (DDR_DDR_DQ_MAP0/1/2/3) have to be properly set.

I cannot figure out how to set these from the TRM, as it is minimal in description.

Any more explanation or example you can provide would be great.

Thank you

Trevor

T1042DQMemory DQ
024
126
228
327
425
531
630
729
840
946
1042
1143
1247
1341
1444
1525
1616
1717
1823
1919
2020
2118
2222
2321
2448
2552
2651
2750
2849
2954
3053
3155
3266
3369
3468
3563
3662
3767
3864
3965
408
4112
4210
439
4415
4514
4613
4711
480
493
504
512
521
535
546
557
5656
5757
5862
5963
6060
6161
6258
6359
D1_MECC032
D1_MECC134
D1_MECC235
D1_MECC338
D1_MECC439
D1_MECC536
D1_MECC633
D1_MECC737
7 Replies

327 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello 
@trevorfox 

Hope this post finds you well,

Could you please be so kind to provide us with your CodeWarrior logs/screenshot errors?

Could you please also provide us with your CodeWarrior version and your current OS?

We will be aware for your kind reply.

Have a great day.

Best Regards,

Hector Villarruel S

0 Kudos
Reply

307 Views
trevorfox
Contributor III

Hi

Codewarrior for PA, v10.5.1

QCVS Rev 4.5

Windows 10

 

I have attached the screenshot of the error. This only happens on one board, the other one seems to work fine.

0 Kudos
Reply

302 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @trevorfox 

Hope this post finds you well,

We notice that you create a technical support ticket,

We will keep the communication on #00681961

Have a great day.

BR,

Hector Villarruel S

0 Kudos
Reply

273 Views
trevorfox
Contributor III
Hi Hector,
I posted on the support case/ticket #00681961 but have not yet heard anything. Do you know of any updates?

262 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @trevorfox 

Hope this post finds you well,

There is an update available on case #00681961 

Kindly keep the communication on such case.

Have a great day.

BR,

Hector Villarruel

0 Kudos
Reply

186 Views
trevorfox
Contributor III

Hi @Hector_Villarruel Hector,

I have posted a response to your post on the support ticket, 00681961. Do you have any updates?

 

Trevor

Tags (1)

164 Views
Hector_Villarruel
NXP TechSupport
NXP TechSupport

Hello @trevorfox 

Hope this post finds you well,

I have sent you an update from on the ticket #00681961

Kindly keep the communication on #00681961

Thank you for your understanding.

Have a great day.

BR,

Hector Villarruel

0 Kudos
Reply