Hi,
I have a custom board that I have received four of. It has a T1042 with attached DDR3L memory, 72 bit data bus.
Three of the four boards has functional DDR, the fourth is intermittent failures when SW loads the DDR. I am trying to use the NXP Codewarrior QCVS DDR validation tool but it is failing initialization, and I recall from another project that due to the data bits being swizzled on some of the byte lanes, the DQ mapping registers (DDR_DDR_DQ_MAP0/1/2/3) have to be properly set.
I cannot figure out how to set these from the TRM, as it is minimal in description.
Any more explanation or example you can provide would be great.
Thank you
Trevor
T1042DQ | Memory DQ |
0 | 24 |
1 | 26 |
2 | 28 |
3 | 27 |
4 | 25 |
5 | 31 |
6 | 30 |
7 | 29 |
8 | 40 |
9 | 46 |
10 | 42 |
11 | 43 |
12 | 47 |
13 | 41 |
14 | 44 |
15 | 25 |
16 | 16 |
17 | 17 |
18 | 23 |
19 | 19 |
20 | 20 |
21 | 18 |
22 | 22 |
23 | 21 |
24 | 48 |
25 | 52 |
26 | 51 |
27 | 50 |
28 | 49 |
29 | 54 |
30 | 53 |
31 | 55 |
32 | 66 |
33 | 69 |
34 | 68 |
35 | 63 |
36 | 62 |
37 | 67 |
38 | 64 |
39 | 65 |
40 | 8 |
41 | 12 |
42 | 10 |
43 | 9 |
44 | 15 |
45 | 14 |
46 | 13 |
47 | 11 |
48 | 0 |
49 | 3 |
50 | 4 |
51 | 2 |
52 | 1 |
53 | 5 |
54 | 6 |
55 | 7 |
56 | 56 |
57 | 57 |
58 | 62 |
59 | 63 |
60 | 60 |
61 | 61 |
62 | 58 |
63 | 59 |
D1_MECC0 | 32 |
D1_MECC1 | 34 |
D1_MECC2 | 35 |
D1_MECC3 | 38 |
D1_MECC4 | 39 |
D1_MECC5 | 36 |
D1_MECC6 | 33 |
D1_MECC7 | 37 |
Hello
@trevorfox
Hope this post finds you well,
Could you please be so kind to provide us with your CodeWarrior logs/screenshot errors?
Could you please also provide us with your CodeWarrior version and your current OS?
We will be aware for your kind reply.
Have a great day.
Best Regards,
Hector Villarruel S
Hello @trevorfox
Hope this post finds you well,
We notice that you create a technical support ticket,
We will keep the communication on #00681961
Have a great day.
BR,
Hector Villarruel S
Hello @trevorfox
Hope this post finds you well,
There is an update available on case #00681961
Kindly keep the communication on such case.
Have a great day.
BR,
Hector Villarruel
Hi @Hector_Villarruel Hector,
I have posted a response to your post on the support ticket, 00681961. Do you have any updates?
Trevor
Hello @trevorfox
Hope this post finds you well,
I have sent you an update from on the ticket #00681961
Kindly keep the communication on #00681961
Thank you for your understanding.
Have a great day.
BR,
Hector Villarruel