DDR Single-Bit ECC QorIQ T1040

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR Single-Bit ECC QorIQ T1040

943 Views
alexcherniakov
Contributor I

Section 14.4.77 in T1040 Reference Manual:

In DDR_ERR_SBE register, if SBET is set to 0, then what could be expected in SBEC field? Does it count the single-bit errors? Please advice. The register description is attached.

Labels (1)
0 Kudos
Reply
1 Reply

825 Views
ufedor
NXP Employee
NXP Employee

The ERR_SBE[SBEC] will be incremented, error event in the ERR_DETECT[SBE] will be triggered after the ERR_SBE[SBEC] overflow (0xFF->0x00).