Compiling U-Boot in 32 bit mode for T2080 QDS board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Compiling U-Boot in 32 bit mode for T2080 QDS board

2,002 Views
manishraturi
Contributor I

Hi Team,

We are using T2080QDS reference board as a base for developing our customized board. When I see the memory map of the reference board, all the addresses are provided in 36 bit. But as our OS support 32 bit addressing. We want U-Boot also to use 32 bit addressing. Keeping this in mind we prepared a memory map( Attached with this email). Now I have some confusion about these macros below:

=====================================

Reference board macro's for PCIE controller 1

=====================================

/* controller 1, direct to uli, tgtid 3, Base address 20000 */

#define CONFIG_SYS_PCIE1_MEM_VIRT       0x80000000

#define CONFIG_SYS_PCIE1_MEM_BUS        0xe0000000

#define CONFIG_SYS_PCIE1_MEM_PHYS       0xc00000000ull

#define CONFIG_SYS_PCIE1_MEM_SIZE       0x20000000      /* 512M */

#define CONFIG_SYS_PCIE1_IO_VIRT        0xf8000000

#define CONFIG_SYS_PCIE1_IO_BUS         0x00000000

#define CONFIG_SYS_PCIE1_IO_PHYS        0xff8000000ull

#define CONFIG_SYS_PCIE1_IO_SIZE        0x00010000      /* 64k */

As I see from the above macro definition the MEM_PHYS is 36 bit and the MEM_VIRT(TLB )entry is 32 bit virtual address and MEM_BUS is again 32 bit address , which according to my understanding overlap with the DDR memory map address(But I think as the reference board maps 2GB DDR only in U-BOOT that should be fine).

If I want to change the above macros according to our memory map(attached with this email), then will the below definition below will work:

/*For SVC */

#ifdef SVC_PCIE1

#define CONFIG_SYS_PCIE1_MEM_VIRT       0xC0000000

#define CONFIG_SYS_PCIE1_MEM_BUS        0xC0000000

#define CONFIG_SYS_PCIE1_MEM_PHYS       0xC00000000ull

#define CONFIG_SYS_PCIE1_MEM_SIZE       0x10000000      /* 256M */

#define CONFIG_SYS_PCIE1_IO_VIRT        0xE0000000

#define CONFIG_SYS_PCIE1_IO_BUS         0x00000000

#define CONFIG_SYS_PCIE1_IO_PHYS        0xE00000000ull

#define CONFIG_SYS_PCIE1_IO_SIZE        0x00010000      /* 64k */

#endif

Please help in entering the correct values for these macros according to our memory map.

Thanks & Regards

Manish Raturi

Labels (1)
0 Kudos
Reply
1 Reply

1,739 Views
bpe
NXP Employee
NXP Employee

CONFIG_SYS_PCIE?_MEM_BUS macro defines the base address of the region

as it is seen on the PCI bus. This macro is used in PCIe ATMU initialization,

the size of the corresponding bus address depends on CONFIG_SYS_PCI_64BIT, see include/pci.h

The base address of the bus region as seen by the local

CPUs is defined by CONFIG_SYS_PCIE?_MEM_PHYS. Therefore, you cannot

eliminate any overlap in the local memory map  by playing with

CONFIG_SYS_PCIE?_MEM_BUS macro.

If the question is,  if a ready configuration for u-Boot with all

peripherals mapped to physical addresses below 4G exists, the answer

is no.  To see if your configuration is valid, try it on your board.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply