Are there any plans to design a heterogeneous single core processor?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Are there any plans to design a heterogeneous single core processor?

1,233件の閲覧回数
christianhehn
Contributor I

Is the a single core QorlQ processor with the same number of transistors as a multicore processor?  Other than statically allocated cores of a multicore, such a heterogeneous single core processor would field flexible and dynamically allocated regions in the processor that are able to independently perform computing tasks as a multicore does (concept is partially implemented by certain GPUs, I suppose), i.e. such regions would not be statically bounded like those of the current QorlQ processors. That way only really the transistors required would be switched on and the memory usage would be more optimally, I suppose.

ラベル(1)
0 件の賞賛
返信
1 返信

1,016件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hi,

This is good concept. I am not aware of that. I think road map related information may be not public.

Regards

0 件の賞賛
返信