Anyone got the mmc working with 8 bit width?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Anyone got the mmc working with 8 bit width?

1,630 Views
ronbelaire
Contributor II

Best I can get is 4 bit width.  Looks like MMC_CAP_BUS_WIDTH_TEST is not set and then mmc_compare_ext_csds() fails.

This is on a T4240 running Linux 3.14.

0 Kudos
Reply
1 Reply

1,494 Views
Pavel
NXP Employee
NXP Employee

Check the rtsx_pci_sdmmc.c file this file contains the MMC_CAP_BUS_WIDTH_TEST setting.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply