Anyone got the mmc working with 8 bit width?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Anyone got the mmc working with 8 bit width?

1,597 次查看
ronbelaire
Contributor II

Best I can get is 4 bit width.  Looks like MMC_CAP_BUS_WIDTH_TEST is not set and then mmc_compare_ext_csds() fails.

This is on a T4240 running Linux 3.14.

0 项奖励
回复
1 回复

1,461 次查看
Pavel
NXP Employee
NXP Employee

Check the rtsx_pci_sdmmc.c file this file contains the MMC_CAP_BUS_WIDTH_TEST setting.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复