Addressing NOR and NAND Flash on the T2080 using ADM mode 0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Addressing NOR and NAND Flash on the T2080 using ADM mode 0

Jump to solution
2,441 Views
Larry5335
Contributor IV

Customer is using NOR Flash as the primary boot device and then switching over to raw NAND Flash. The driver being used for the NAND requires 4 Ready/Busy hardware lines, 1 for each of the physical Flash components. To set this up in the pin muxing, it looks like IFC_A29:31 become IFC_RB2:4 and these pins are no longer available for NOR Flash addressing.

Is this correct?

What is the largest NOR device that can be addressed assuming IFC_A29:31 are not available and used as RB2:4?

i.e. will using ADM mode 0 with a shift of 3 allow the use of a 2 ** 29 - 512 Mbit NOR Flash or is there some other limit?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,929 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes IFC_RB2:4 and IFC_A29:31 share 3 pins and if we need for any of IFC_RB2:4 then we lose IFC_A29:31. It is selected in the RCW[IFC_GRP_B].

In the ADM mode 0 (ADM_SHFT_MODE=0) IFC_A29:31 provide 3 least significant address bits irrespective of the ADM_SHFT value. There are not other pins where we can get these 3 lsb. So without IFC_A29:31 we can address 64-bit word only in the ADM mode 0. At the same time we can read 16-bit only through IFC_AD[0:15]. Hence it is not good for parallel NOR flash. I think you should consider using ADM_SHFT_MODE=1 when IFC_AD bus will carry lsbs and IFC_A bus carries the msb.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,929 Views
zhylunwen
Contributor I

hello,Serguei Podiatchev,does t2080 support datasheet figure 13-8?  This is a bug for t2080?

0 Kudos
Reply
1,929 Views
r8070z
NXP Employee
NXP Employee

Yes there is mispint in the T2080 manual figure 13-28. The IFC_A[26] cannot provide the least significant bit of byte address.

0 Kudos
Reply
1,930 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

Yes IFC_RB2:4 and IFC_A29:31 share 3 pins and if we need for any of IFC_RB2:4 then we lose IFC_A29:31. It is selected in the RCW[IFC_GRP_B].

In the ADM mode 0 (ADM_SHFT_MODE=0) IFC_A29:31 provide 3 least significant address bits irrespective of the ADM_SHFT value. There are not other pins where we can get these 3 lsb. So without IFC_A29:31 we can address 64-bit word only in the ADM mode 0. At the same time we can read 16-bit only through IFC_AD[0:15]. Hence it is not good for parallel NOR flash. I think you should consider using ADM_SHFT_MODE=1 when IFC_AD bus will carry lsbs and IFC_A bus carries the msb.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply