Accessing External interrupt IRQ0 to IRQ11 from Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Accessing External interrupt IRQ0 to IRQ11 from Linux

1,388 Views
shrikantkumar
Contributor I

We are trying to access external interrupt IRQ0 to IRQ11 using Linux. What is the configuration required in uboot/DTS/Linux to test the external interrupts?

Labels (1)
0 Kudos
Reply
3 Replies

1,352 Views
shrikantkumar
Contributor I

The given solution is for layerscape processors. The same wont be applicable for Powerpc based processor.

0 Kudos
Reply

1,340 Views
Oswalag
NXP TechSupport
NXP TechSupport

It has information about how to manage the interrupts in linux (any device), the configuration of the external IRQ's is available in the RM (Polarity, Sense, Priority, etc.)

0 Kudos
Reply

1,369 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

You can refer to the following thread in the community:

how to use IRQ0~11 in kernel?

BR.

0 Kudos
Reply