linker error "The TEXT sections are larger than the limit supported by the license for this linker."

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

linker error "The TEXT sections are larger than the limit supported by the license for this linker."

1,387 次查看
supriyapatil
Contributor I

Hello

 

Please help me to resolve link error as

The TEXT sections are larger than the 524288 byte limit supported by the license for this linker.

 

Is there any compiler settings or i need to upgrade CW?

 

Please let me know

 

thanks

supriya

标签 (1)
0 项奖励
回复
1 回复

1,095 次查看
trytohelp
NXP Employee
NXP Employee

Hi Supriya,

It seems you reached the code size limit.

Difficult to provide you more info but following the message generated by the linker it should be a license issue.

I recommend to have a look to the link:

      http://www.freescale.com/webapp/sps/site/overview.jsp?code=CW_SUITES&tid=CWH

At left side select the product you're looking for.

At right side you will have info for  4 suites (Special, Basic, Standard and Professional).


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复