can I use CodeWarrior after registration expires?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can I use CodeWarrior after registration expires?

Jump to solution
1,341 Views
danielmilutinov
Contributor III

Hi,

 

I am programming in assembly and my CodeWarrior 30-day evaluation period is about to expire. My understanding is that I can continue to use CodeWarrior after the 30 period and don't need to do anything, even though the pop-up screen says I can use CodeWarrior until the current license expires. 

 

Please confirm.

 

Dan

Labels (1)
0 Kudos
Reply
1 Solution
1,218 Views
danielmilutinov
Contributor III

CodeWarrior continues to function normally after the 30-day evaluation period, so there is no need to register. 

View solution in original post

0 Kudos
Reply
2 Replies
1,218 Views
stanish
NXP Employee
NXP Employee

Hello Daniel,

Not sure which CodeWarrior you are using.

Usually after the evaluation period expires it is automatically switched to free Special Edition (if such version exists) so you don't have to register it.

Stan

0 Kudos
Reply
1,219 Views
danielmilutinov
Contributor III

CodeWarrior continues to function normally after the 30-day evaluation period, so there is no need to register. 

0 Kudos
Reply