can I use CodeWarrior after registration expires?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

can I use CodeWarrior after registration expires?

ソリューションへジャンプ
1,460件の閲覧回数
danielmilutinov
Contributor III

Hi,

 

I am programming in assembly and my CodeWarrior 30-day evaluation period is about to expire. My understanding is that I can continue to use CodeWarrior after the 30 period and don't need to do anything, even though the pop-up screen says I can use CodeWarrior until the current license expires. 

 

Please confirm.

 

Dan

ラベル(1)
0 件の賞賛
返信
1 解決策
1,337件の閲覧回数
danielmilutinov
Contributor III

CodeWarrior continues to function normally after the 30-day evaluation period, so there is no need to register. 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,337件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello Daniel,

Not sure which CodeWarrior you are using.

Usually after the evaluation period expires it is automatically switched to free Special Edition (if such version exists) so you don't have to register it.

Stan

0 件の賞賛
返信
1,338件の閲覧回数
danielmilutinov
Contributor III

CodeWarrior continues to function normally after the 30-day evaluation period, so there is no need to register. 

0 件の賞賛
返信