Rehost Code Warrior license

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Rehost Code Warrior license

1,629 次查看
TomasH
Contributor I

I get this exception when I try to rehost one of my CW licenses.

 

------------

The call to lmcrypt failed.

Tried to invoke method public java.lang.String GenerateLMCryptLicense.generate(java.lang.String,java.lang.String) throws java.lang.Exception with arguments java.lang.String,java.lang.String.  The arguments do not match the signature.; nested exception is: java.lang.IllegalArgumentException: java.lang.ClassCastException@71a97

----------

 

I have done the same thing many times before. I usually use the MAC address, but I tried both the network address and the drive volume id.

Both threw a java exception.

标签 (1)
0 项奖励
回复
3 回复数

1,412 次查看
trytohelp
NXP Employee
NXP Employee

Hi Tomas,

Do you have the problem with the web system ?

In our data base under your account I've found several registrations.

Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,412 次查看
TomasH
Contributor I

I treied several times yesterday, and with different browsers (IE and Crome). It didn't work. Same error message as the other two guys.

Can't generate Key for CW. Get message...

Lmcrypt error when generation CW key

But today it worked and I could generate a key. Close this issue.

/T

0 项奖励
回复

1,412 次查看
trytohelp
NXP Employee
NXP Employee

thanks for the info.


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复