[Q] v11.0 C++ build error with Prof. license

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[Q] v11.0 C++ build error with Prof. license

1,293 次查看
jongcheonkim
Contributor II

Hello. I have CodeWarrior Prof. license

I tested with CodeWarrior for MCU v11.0

- C++ project with Volume ID license generate: no problem

- C++ project with USB Dongle ID license generate: 'C++ is not supported by the current set of licenses and is disabled.'

  error happen.

(I checked license activate via CodeWarrior and LMTOOLS both)

- C project: no problem regardless of Volume ID/USB Dongle ID license

For CW to v10.7 with same USB Dongle.

I have no problem C++ project - license gen via Dongle ID

What do I need to check to use CW v11.0 via Dongle License?

Best Regards,

Mac.

0 项奖励
回复
1 回复

1,175 次查看
jongcheonkim
Contributor II

Hello.

I accidentally pressed the 'assumed answer' button, but this issue has not been resolved yet. ;-(

If you know the solution, please answer it.

Best Regards,

Mac.

0 项奖励
回复