Licensing for CW10.1 Special Edition for Kinetis

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Licensing for CW10.1 Special Edition for Kinetis

跳至解决方案
3,595 次查看
Niall
Contributor II

When I try to build a project in CW10_MCU_V10.1_SE I get a message saying my application could not obtain a license file. I though that the special edition did not require a license file.

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
1,859 次查看
jorge_plascencia
NXP TechSupport
NXP TechSupport

Sorry for the late reply on this topic.

This issue is a known issue specific to the Kinetis build tools (therefore, only people building with those targets should experience this issue).  It will be addressed in future releases.

In the meantime, here is the best workaround:

Edit the "cwide-env" file which is located at: {install path}\eclipse\

Append the following line to the file (just use a text editor):

FLEXLM_BATCH= -add 1

在原帖中查看解决方案

0 项奖励
回复
7 回复数
1,860 次查看
jorge_plascencia
NXP TechSupport
NXP TechSupport

Sorry for the late reply on this topic.

This issue is a known issue specific to the Kinetis build tools (therefore, only people building with those targets should experience this issue).  It will be addressed in future releases.

In the meantime, here is the best workaround:

Edit the "cwide-env" file which is located at: {install path}\eclipse\

Append the following line to the file (just use a text editor):

FLEXLM_BATCH= -add 1

0 项奖励
回复
1,859 次查看
joker441
Contributor I

same here...

0 项奖励
回复
1,859 次查看
Niall
Contributor II

I would like to add some more information on my previous post. I have installed the Special Edition of CW10.1 for windows (CW10_MCU_V10.1_SE). When I try to build one of the Kinetis example projects I get a Flexnet License Finder error saying that a license can't be obtained. The screenshot is attached. My understanding is that the Special edition of Codewarrior does not need a registered license and that a license file is installed during installation. My installation directory does not contain a license.dat file.

 

Has anybody else come across the same problem? I am trying to figure out if it is an installation problem or a bug in the special edition.

0 项奖励
回复
1,859 次查看
moat
Contributor I

error still exists...

 

Downloading eval now.

0 项奖励
回复
1,859 次查看
kef
Specialist I

Did you see last post to this thread ?:

https://community.freescale.com/thread/80580

0 项奖励
回复
1,859 次查看
olebon
Contributor I

I am having the same problem. I guess it will never be solved :smileysad: The only solution is to remove this retarded CW and use IAR instead.

 

 

PS Just added "FLEXLM_BATCH= -add 1" to the eclipse config file, this helped. Decided to keep CW :smileyhappy:

0 项奖励
回复
1,859 次查看
emh203
Contributor II

I have experienced this too.   I amusing the evaluation edition for now....

0 项奖励
回复