I3C slave ip

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,264件の閲覧回数
chengxiaolei
Contributor I

I'm using the free NXP I3C slave IP (https://www.nxp.com/webapp/sps/download/preDownload.jsp ) and find it's very helpful, but i have some questions about it  following :

 I need to use the master model to verify the I3C slave that is designed by your company investor, Is there an official I3C master model simulation ?

  there is not a tst_i3c_master_model.v in the free NXP I3c slave IP, but it is uesed in simulation file; can you provide it for me ?

 

Thanks and best regards,

ethan

タグ(1)
0 件の賞賛
返信
1 解決策
3,164件の閲覧回数
64640344
Contributor I

tst_i3c_master_model.v is NOT provided with the I3C_NXP_Free_License_Slave.zip .

Could you add the file into I3C_NXP_Free_License_Slave.zip and update  I3C_NXP_Free_License_Slave.zip.

Thank you.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,165件の閲覧回数
64640344
Contributor I

tst_i3c_master_model.v is NOT provided with the I3C_NXP_Free_License_Slave.zip .

Could you add the file into I3C_NXP_Free_License_Slave.zip and update  I3C_NXP_Free_License_Slave.zip.

Thank you.

0 件の賞賛
返信