I hold a license for the CodeWarrior IDE for Mac OS X

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I hold a license for the CodeWarrior IDE for Mac OS X

1,520 次查看
christianhehn
Contributor I

CodeWarrior™ Development Studio for Mac ® OS

 

 

CodeWarrior C/C++ Compiler for Mac OS X/PPC.

Copyright (c)2005 Freescale Semiconductor, Inc.

All rights reserved.

Version 4.1 build 448

Runtime Built: Oct 24 2005 12:01:32

 

Hardware :

  Modelnavn:    Mac mini

  Model-id:    PowerMac10,1

  Processornavn:    PowerPC G4  (1.2) PowerPC 7450

  Processorhastighed:    1.25 GHz

  Antal CPU'er:    1

  L2-buffer (pr. CPU):    512 KB

  Hukommelse:    1 GB

  Bushastighed:    167 MHz

 

9.8.0 Darwin Kernel Version 9.8.0: Wed Jul 15 16:57:01 PDT 2009; root:xnu-1228.15.4~1/RELEASE_PPC Power Macintosh

when i type mwcc pq.c -o pq

 

I get

Warning : Environment varibale 'MWCIncludes' not found

Warning : Environment variable 'MWLibraries' not found

     Error : License check fialed: No such feature exists

                Feature:        MacOS_Plugins_MacOSX_Limited

                License path: /Volumes/CW Tools 10.0/Metrowerks CodeWarrior 10.0/

                Metrowerks -

                       CoderWarrior/license.dat

                FLEXlm error: -5,357

                For further information, refer to the FLEXlm End User Manual,

        available at "www.macrovision.com"

 

The second time round having installed the license file, I received by e-mail, something like this came up

 

mwcc pq.c -o pq

Warning : Environment variable 'MWCIncludes' not found

Warning : Environment variable 'MWLibraries' not found

   Error : the file 'stdio.h' cannot be opened

pq.c line 1    #include <stdio.h>

   Error : the file 'math.h' cannot be opened

pq.c line 2    #include <math.h>

 

 

Checking out diverse discussions, someone mentioned that this would be a licensing problem. How do I solve this and get MWCW to work again?? Your help would be greatly appreciated.

标签 (1)
0 项奖励
回复
1 回复

1,168 次查看
TomasPaez
NXP Employee
NXP Employee

I do not see options, MAC Os versions are not being supported by NXP for several years.  

0 项奖励
回复