CodeWarrior dongle license issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior dongle license issue

2,725 Views
junfujimoto
Contributor I

Hi,

When I tried to debug on CodeWarrior 10.7 on Windows 10, I get a error "Download size limit has been exceeded.".(filed_to_resume_target_process.png)

How do I solve this issue?

I assumed this is due to license, then I checked license.dat and lmtools have same FLEXID. (as shown lmtools.png and license.dat.png)

license.dat is located at C:\Freescale\CW MCU v10.7\MCU.

And I get a message "CDE: no license found, using Community Edition License" when I open codewarrior.

Best regards
Jun

0 Kudos
Reply
4 Replies

418 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

Please see the documetn below and the links below. 

Dongle Driver updated: 

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=CWX-FLEX-DD-STD

 

 

Note:

Dongles are no longer supported on Window 10 or 11

0 Kudos
Reply

2,463 Views
TomasPaez
NXP Employee
NXP Employee

Test installing the following drivers option 

https://community.nxp.com/docs/DOC-341008 

0 Kudos
Reply

2,463 Views
junfujimoto
Contributor I

Thanks for your response.

I tried to reinstall dongle drivers as per your advice.

But the issue is still occurred.

no_license_found.png

failed_to_resume_target_process.png

I can see FLEXID on lmtools.

Does this mean I've installed drivers correctly?

lmtools.png

And I get this result when I run haspdinst.exe -info.

This shows akspccard.sys is not installed. Is it no problem?

haspdinst_info.png

0 Kudos
Reply

952 Views
hanbinbyun
Contributor I

Did you solve the above problem?

 

"CDE: no license found, using Community Edition License"

Even if there's a phrase above, I haven't found any problems with compilation and debugging until now, but did you have any problems while doing it?

0 Kudos
Reply