Code Warior 10.6 Evaluation Version" license expired revert to Special Edition?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code Warior 10.6 Evaluation Version" license expired revert to Special Edition?

Jump to solution
717 Views
whw
Contributor I

I installed "Code Warior 10.6 Evaluation Version" whose license is now expired. I now need only the "Special Version".

 

Questions 1: Does the CW 10.6 Evaluation Version revert to Special Version on expiry?

Question 2: If answer to question 1 is YES, how to turn off the warning that CW is expired that appears every time CW is started?

 

Thanks

Labels (1)
0 Kudos
Reply
1 Solution
532 Views
trytohelp
NXP Employee
NXP Employee

Hi,

Without license file the tool (CW for MCU V10.x) is working at Special Edition level.

As you used an evaluation one, a temporary license file was included.

This license should be located under the folder: \CW MCU v10.6.4\MCU.

You can rename the license file as license.dat_.

Now the message will not appear anymore.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
533 Views
trytohelp
NXP Employee
NXP Employee

Hi,

Without license file the tool (CW for MCU V10.x) is working at Special Edition level.

As you used an evaluation one, a temporary license file was included.

This license should be located under the folder: \CW MCU v10.6.4\MCU.

You can rename the license file as license.dat_.

Now the message will not appear anymore.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply