Client computer not able to obtain CW license from the Server

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Client computer not able to obtain CW license from the Server

ソリューションへジャンプ
2,910件の閲覧回数
rhagberg
Contributor I

I have set up a floating license for Code Warrior on our license server at work, and it seems to be up and running. When I start Code Warrior it tries to obtain a license from the server, but never get's a response. I have used wire shark on both the client and the server and can see the request going to the server, but the server never responds.  I have set up the firewall on the server to allow TCP and UDP from the client to pass through, and still no response. Eventually Code Warrior times out and gives me the following error messages. I would appreciate any help as I am unsure of what to try next. Thank you.

CWLicenseErrors.PNG

0 件の賞賛
返信
1 解決策
2,835件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Can you help me perform the steps below:

 

Server Side:

  1. Can you send me the logs
  2. Open a CMD and go to the location where theFlexLM is hosted
  3. Run the command lmgrd -z
  4. Please send me a screen capture of the result

Client Side:

  1. open a CMD and do a telnet to the server with the port number eg. 128.0.0.0  2700
    1. send me a screen capture of the result

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,836件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Can you help me perform the steps below:

 

Server Side:

  1. Can you send me the logs
  2. Open a CMD and go to the location where theFlexLM is hosted
  3. Run the command lmgrd -z
  4. Please send me a screen capture of the result

Client Side:

  1. open a CMD and do a telnet to the server with the port number eg. 128.0.0.0  2700
    1. send me a screen capture of the result
0 件の賞賛
返信