How to install/use USBdongle license under Win 8.1? (Include test with CW for MPC55xx V2.7 & CW for HC12 v5.1)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to install/use USBdongle license under Win 8.1? (Include test with CW for MPC55xx V2.7 & CW for HC12 v5.1)

How to install/use USBdongle license under Win 8.1? (Include test with CW for MPC55xx V2.7 & CW for HC12 v5.1)

How to install/use USBdongle license under Win 8.1?

 

 

Configuration used:

                Native installation Win 7 Enterprise 64 bit

                Oracle VM VirtualBox V4.3.28 r 100309

                                Windows 8.1 Enterprise 64 bit

 

 

This doc will answer the question:

            Can we use USBdongle license under Win 8.1 ?

 

There are 2 parts:

  • - How to install the Dongle driver and check it ?
  • - How to use a development tool with USBdongle license file under Win8.1 ?

 

 

Attached you will find 2 videos explaining the processes.

 

  • - How to install the Dongle driver and check it ?

Refer to the USBDongle_driver_installation.avi

     BEFORE Phase 4, to avoid problem we recommend to un-plug ethernet cable or switch-off wifi.

     If network connection is not switched-off, for Phase 4 and Phase 5, a wrong driver could be installed.

 

              Right Driver version (USBDongle + FlexID Driver installed + Windows 7 64bit)

  107951_107951.pngpastedImage_3.png

 

  • - How to use a development tool with USBdongle license file under Win8.1 ?

To test it I used:

     -  CW for MPC55XX V2.7

          Refer to the USBDongle_win8_MPC55XX.avi

                              - CW for HC12 V5.1

                                   Refer to the USBDongle_win8_hc12v5.1.avi

                                    Include example project -> HC12_V5_1_test_project.zip

 

Hope this will help.

Pascal

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎06-12-2015 02:55 AM
更新者: