Floating License -Environment Variables.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Floating License -Environment Variables.

Floating License -Environment Variables.

1. Download service manager.

2. License Manger update

  • If your license manager have the following view, an update is needed.
    • pastedImage_7.png
  • Updated License Manager view
    • pastedImage_8.png

In the previous links the updated License Manager can be downloaded.

3. Open LM Tools / Go to Config Services tab pastedImage_13.png

  1. Service Name: Please type a new service name.
  2. Service Name: Please type a new service name.
  3. Path to the license: select the location of the license file.
  4. Path to log file: create a file to save the log file from server.
  5. Uncheck Start Server at power-up.
  6. Check Use Service.

4. Open Start/Stop/Reread tab

  • Select the new created service and click on reread License file.
  • Check on the license status on the low left side of the windows. License read successfully is expected.pastedImage_19.png

5. License path information

  • Review the license.dat file in in the installation path location. Make sure you have the same copy that holds the server, so the serve information referenced in license.dat file can be the same.
  • Classic CodeWarrior IDE, save the license.dat file in the directory where you installed the software
    • (usually C:\Program Files\NXP\Code Warrior for XYZ\).
  • Eclipse IDE, save the license.dat file in the directory where you installed the software
    • (usually C:\Program Files\NXP\CW XYZ v10.x\XZY\license.dat).
  • CodeWarrior for Networking
    • C:\Freescale\CW4NET_v2018.01\Common 

6. How to set an environment variable pastedImage_24.png

  • Go to System within control panel.
  • Click on advanced system settings.
  • Go to Environment Variables.
  • Look for METROWKS_LICENSE_FILE – if there is no variable please click on add.
  • Assign value to for client
  • Classic CodeWarrior IDE, save the license.dat file in the directory where you installed the software (usually C:\Program Files\NXP\Code Warrior for XYZ\).
  • Close and test
附件
评论

Hello

Thanks for the complete documentation.

I have a question here-

1.  When I install the License Manager for Windows, LMtools.exe also gets installed inside the FLex_LM folder.But it needs admin rights to run the application.

2. Also, a separate link for LMTools.exe is given-

Thanks

Admin_rights.jpeg

The error message that you are getting is due to an update on Windows 10, you can use the 64bit and it will still work as expected.

Regards,

无评分
版本历史
最后更新:
‎09-02-2019 10:45 AM
更新人: