What happens when the maximum number of allowed authentication attempts is reached?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What happens when the maximum number of allowed authentication attempts is reached?

Jump to solution
818 Views
psvz
Contributor IV

From Documentation

SE050 APDU Spec:
3.2.1.9 UserID
... By default, the maximum number of allowed authentication attempts is set to 255.

and APIs such as

smStatus_t Se05x_API_WriteUserID(pSe05xSession_t session_ctx,
    pSe05xPolicy_t policy,
    SE05x_MaxAttemps_t maxAttempt,...

So, what exactly will happen on my SE051H if I set number of max attempts to, say, 5 and then exceed it? Does it count unsuccessful attempts only or *all* attempts?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
783 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @psvz ,

 

Yes, it counts unsuccessful authentication attempts.  Please kindly refer to the following for details.

Kan_Li_0-1746683118201.png

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

View solution in original post

0 Kudos
Reply
1 Reply
784 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @psvz ,

 

Yes, it counts unsuccessful authentication attempts.  Please kindly refer to the following for details.

Kan_Li_0-1746683118201.png

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply