we have a customer use Desfire EV3, They ask the maximum input voltage of LA/LB , this parameter I did not find in datasheet. Could you help to check ? thanks a lot
Hi @alina
Theory goes like this...
page 19 in MIFARE DESFire EV3 contactless multi-application IC gives us I-max of 86mA.
In a resonant LC circuit voltages on L and C are misaligned. I assume the ask comes from the need to assess calibrating capacitor rating, so let's deal with Vc.
VCmax = Imax * XC (capacitive reactance)
XC = 1 / (2 * π * f * C)
Assuming values 13.56MHz and 70pF, VCmax = 14.4V
I don't believe it is possible to guarantee anything here because an external reader outside your control drives the voltage - hence it can't be part of the specs.