Are there any plans to support mbedtls3.X in SE05x-MW-v04.XX.XX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are there any plans to support mbedtls3.X in SE05x-MW-v04.XX.XX

Jump to solution
1,642 Views
Xiao8Chongxu
Contributor II

currently only support mbedtls 2.26.0

Xiao8Chongxu_0-1679883291675.png

 

Labels (1)
Tags (1)
0 Kudos
1 Solution
1,631 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Xiao8Chongxu ,

 

mbedtls3.X will be supported in the future, do you have any urgent cases need this feature? is it possible to give us more details?

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
6 Replies
1,632 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Xiao8Chongxu ,

 

mbedtls3.X will be supported in the future, do you have any urgent cases need this feature? is it possible to give us more details?

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
58 Views
Xiao8Chongxu
Contributor II

hi, really a long time..

can i get the V3.X solution now days?

it is really an emergency.

0 Kudos
1,625 Views
Xiao8Chongxu
Contributor II

HI, Kan

My products have selected SE051 as secure basement, and been planned to release before the end of 2024.

Currently, mbedtls 3.0 has been integrated as crypto library and can not changing-over to version2.*.

During prototype verification with OM-SE051ARD, I encountered this version issue.

------------

will mbedtls3.X adaptation meets us soon within this year 2023?

 

really Thks for your reply.

 

 

0 Kudos
1,618 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @Xiao8Chongxu ,

 

Thanks for the information! I will forward to our product management later. BTW, is there any Disti/NXP FAE following up with your project? 

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
1,613 Views
Xiao8Chongxu
Contributor II

really great!!, openssl 3.X and mdedtls 3.X are wildly used later on.

0 Kudos
1,623 Views
Xiao8Chongxu
Contributor II

Supplementary notes:

My company's open source strategy: we are as much as possible not to modified ext library, like your SE05x-MW-v04.XX.XX.

Tags (1)
0 Kudos