related to CDK tool output frame

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

related to CDK tool output frame

1,432 Views
Pranav_Tonape
Contributor I

HI NXP team,

for TPMS RF  application we are using NXP NTM88 ic as a transmitter where as NXP lizard V2 board as a receiver, 

in attached image i have a question

1) i was changed payload length 18 in a code but it still show 12, why? or that 12 has another meaning in the CDK tool

2) the z Coolum having a data 80 and C0 what is that? and what is an write value 80 or C0?

please help me out from it

 

tanks and regards,

Pranav Tonape

  

Labels (1)
0 Kudos
Reply
1 Reply

1,388 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Pranav, 

1. Is data in column H displayed in hexa or decimal? Because 0x12 = 18. So, if data is displayed in hexa, it corresponds to a payload length of 18 bytes.

2. These are code violation bits. They are explained in the AN13717.

BR, Tomas

 

 

0 Kudos
Reply