pressure sensor MPXV7002 temperature range

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

pressure sensor MPXV7002 temperature range

Jump to solution
1,701 Views
andreacelani
Contributor II

The pressure sensor MPXV7002 has following temperature ranges:

operating: TA +10...+60°C

Do may cause permanent damage if operating at -10°C...+9°C? [yes or no]

I can accept in my project that the error will increase outside of the compensated temperature range (+10...+60°C), but I cannot accept that the sensor will be permanent damaged, as stated in the datasheet (Table 4. Maximum Ratings, note [1]).

Thank you for your help.

0 Kudos
Reply
1 Solution
1,688 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Andrea,

yes, you can use the MPXV7002DP outside of the compensated temperature range (TA +10...+60°C), from -30°C to 100°C without damage. But as you mentioned the error is increased outside of the compensated area and we cannot guarantee how much.

With Best Regards,

Jozef

View solution in original post

0 Kudos
Reply
1 Reply
1,689 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Andrea,

yes, you can use the MPXV7002DP outside of the compensated temperature range (TA +10...+60°C), from -30°C to 100°C without damage. But as you mentioned the error is increased outside of the compensated area and we cannot guarantee how much.

With Best Regards,

Jozef

0 Kudos
Reply