powering FXTH870xD sensor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

powering FXTH870xD sensor

跳至解决方案
1,429 次查看
VictorOsipov
Contributor I

what the best solution to power FXTH870xD sensor from battary?

is it possible to use CR2032 and get life > 1year ?

PS: Sensor used without RF transmitter.

0 项奖励
回复
1 解答
1,392 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Victor,

The choice of the battery has to be made taking into account several parameters like capacity, maximum current peak supported and temperature operating range.

Regarding the capacity, it is common in TPMS applications to use a 120mAh battery and achieve 10 years of battery life. It depends on the wakeup period i.e. the period at which the measurements and RF transmissions are performed.

If you create a standard ticket, I can share with you an Excel file that helps to estimate the power consumption.

Best regards,

Tomas

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,393 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Victor,

The choice of the battery has to be made taking into account several parameters like capacity, maximum current peak supported and temperature operating range.

Regarding the capacity, it is common in TPMS applications to use a 120mAh battery and achieve 10 years of battery life. It depends on the wakeup period i.e. the period at which the measurements and RF transmissions are performed.

If you create a standard ticket, I can share with you an Excel file that helps to estimate the power consumption.

Best regards,

Tomas

0 项奖励
回复
1,379 次查看
VictorOsipov
Contributor I

case 00****84 created, if it is possible - please answer in suitable time with attached document...

thanks!

0 项奖励
回复