nhs3152 simulate a IC card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

nhs3152 simulate a IC card

Jump to solution
1,958 Views
yys3210
Contributor II
i have bought a NHS3152 demo board (E985063)& LPC- LINK2.can I use a IC card reader(14443A support NTAG21x) get the measure datas of nhs3152?
0 Kudos
Reply
1 Solution
1,823 Views
driesmoors
NXP Employee
NXP Employee

Hello,

The NHS3152 IC must run firmware on its Cortex M0+. That application firmware is responsible for configuring the HW blocks, starting an ADC conversion (or temperature, or I2D, or whatever), and using the outcome to create an NDEF message which a tag reader can read out.

The SDK provides a demo application app_demo_dp_tadherence to show how this can be used in a therapy adherence/compliance use case.

Best,
Dries. 

View solution in original post

0 Kudos
Reply
2 Replies
1,823 Views
yys3210
Contributor II

thanks!

0 Kudos
Reply
1,824 Views
driesmoors
NXP Employee
NXP Employee

Hello,

The NHS3152 IC must run firmware on its Cortex M0+. That application firmware is responsible for configuring the HW blocks, starting an ADC conversion (or temperature, or I2D, or whatever), and using the outcome to create an NDEF message which a tag reader can read out.

The SDK provides a demo application app_demo_dp_tadherence to show how this can be used in a therapy adherence/compliance use case.

Best,
Dries. 

0 Kudos
Reply