mpxv7025 sensor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mpxv7025 sensor

2,795 Views
roshank
Contributor II

Can i use mpxv7025 dp pressure sensor with arduino board? 

0 Kudos
Reply
5 Replies

2,590 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Roshan,

Yes, it should be easy to connect this sensor to Arduino boards.

It is a 5V, temperature compensated and calibrated differential pressure sensor for ±25kPa. The offset is 2.5V and the output is 90mV per kPa.

The pins are numbered as follows:

pastedImage_2.png

 

So connect Arduino 5V to sensor pin 2. Arduino GND to sensor pin 3. Arduino analog input (for example A0) to sensor pin 4.

 

Read the analog value and write it to the serial monitor: http://arduino.cc/en/Tutorial/ReadAnalogVoltage

If that is working, you can start to calculate the actual pressure.

Hope it helps!

Best regards,

Tomas

2,590 Views
roshank
Contributor II

Hi tomas,

 I am usinng following circuit. what is the range of ideal ADC

values from pressure sensor.

mpvx7025 dp connection.png

0 Kudos
Reply

2,590 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Roshan,

First off, the operating supply voltage is from 4.75V to 5.25V. 3.3V is out of the recommended range. 

With no pressure applied (no pressure difference between P1 and P2), the output voltage should be around 2.5V. Then try to force some air into P1, e.g. using your mouth and see if the voltage goes up.

Best regards,

Tomas

0 Kudos
Reply

2,590 Views
roshank
Contributor II

Hi tomas,

        Thanks for reply. what is the range of ideal ADC values for inhalation and exhalation for this sensor.

Regards,

Roshan

0 Kudos
Reply

2,590 Views
roshank
Contributor II

Hi tomas,

          I also want to know that when we using this sensor for spirometric project, Is it better to use the sensor directly or with a reference circuit as shown above. which method gives more accuracy.

Regards,

Roshan

0 Kudos
Reply