mc33771C fault

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,763件の閲覧回数
alessandro_piazza
Contributor II

Hi,

I configured GPIO3 to GPIO6 as digital input but UT fault bits in AN_OT_UT_FLT continue to rise (and so in FAULT1_STATUS). I tried to set temp thresholds to min/max but nothing changes. Any help?

thanks!

1 解決策
1,677件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

If no IIC used, the pack controller has to ignore the content of FAULT1_STATUS[I2C_ERR_FLT].

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,688件の閲覧回数
alessandro_piazza
Contributor II

Hi, I've just solved AN_OT_UT_FLT bits (there was an error in the config sequence).

The only alarm I cannot disable remain I2C_ERR_FLT in FAULT1STATUS (I dont use I2C).

Is there any way to disable it?

thanks!

 

0 件の賞賛
返信
1,678件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

If no IIC used, the pack controller has to ignore the content of FAULT1_STATUS[I2C_ERR_FLT].

0 件の賞賛
返信
1,736件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Could you please let me know your configure steps?

 

0 件の賞賛
返信