mag3110 method of calibration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mag3110 method of calibration

ソリューションへジャンプ
3,935件の閲覧回数
2394343453
Contributor I

Dears:

              When I was in debugging mag3110, because our equipment is the on-board equipment, calibration, so unable to manually draw a figure 8 so I want to seek advice, is there any other method of calibration.

BRS

ラベル(1)
0 件の賞賛
返信
1 解決策
3,264件の閲覧回数
anthonyduhamel
NXP Employee
NXP Employee

Hello 大史,

It will be hard to implement the calibration in the hardware because the calibration parameters change depending to the environment. Basically, calibration takes matrix manipulations so integrate it in the firmware. How do you interface with the MAG3110? By the way you can port the calibration to your android project. C & JAVA languages are very closed.

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
3,264件の閲覧回数
anthonyduhamel
NXP Employee
NXP Employee

Hello 大史,

What's your application? What kind of accuracy do you target? We need more information about your project to give you a hand.

Thanks,

Anthony

0 件の賞賛
返信
3,264件の閲覧回数
2394343453
Contributor I

Hello Anthony,

                our  equipment  was installed int the car,  so it can't to draw 8 to calibration.   I know a  circle algorithm,  can you introduced to me?   and  send  the circle algorithm code to me?

                look forward to you apply. 

BRS

0 件の賞賛
返信
3,264件の閲覧回数
anthonyduhamel
NXP Employee
NXP Employee

Hi 大史,

You can have a look at the NXP Sensor Fusion​, we provide a full and open source project for electronic compass.

As the application is embedded in a car, you can NOT run the full 3D compass because you have 2 axis only.

The Sensor Fusion provides different algorithms for electronic compasses and IMUs. In your case, you can use the 2D Automotive Compass which needs a 2D calibration: instead of drawing a 8 it takes only a circle as you mentioned.

sensor fusion.PNG

Code samples are available on our website.

You have to check the

void fRun_3DOF_B_BASIC(struct SV_3DOF_B_BASIC *pthisSV, struct MagSensor *pthisMag, int32 loopcounter, int16 ithisCoordSystem)

function in the fusion.c file.

Anthony

0 件の賞賛
返信
3,262件の閲覧回数
anthonyduhamel
NXP Employee
NXP Employee

大史,

If you want to understand the algorithm, I attached a document about magnetic calibration.

The algorithm is based on an ellipsoid (ellipse in 2D) recognition. When the ellipsoid parameters have been extracted, the algorithm transforms the scattershot  into a sphere (circle in 2D) with mathematical operations.

Capture.PNG

Anthony

0 件の賞賛
返信
3,262件の閲覧回数
2394343453
Contributor I

Hello  Anthony:

                       Thanks for your kind reply.   our  project is android,  where we can set the calibration code,  BSP or HardWare ?

BRS

0 件の賞賛
返信
3,265件の閲覧回数
anthonyduhamel
NXP Employee
NXP Employee

Hello 大史,

It will be hard to implement the calibration in the hardware because the calibration parameters change depending to the environment. Basically, calibration takes matrix manipulations so integrate it in the firmware. How do you interface with the MAG3110? By the way you can port the calibration to your android project. C & JAVA languages are very closed.

0 件の賞賛
返信