how to use ina220 current monitor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to use ina220 current monitor

1,652 Views
odasong
Contributor I

I used the ina220 current monitor by referring to the ls1046frwy document. 

http://www1.futureelectronics.com/doc/NXP/FRWY-LS1046A-TP.pdf 

odasong_4-1697158943647.png

The ina220 current monitor result value is different from what I expected, so I want to modify the ina2xx.c code. According to the QorIQ LS1046A BSP v0.4 document, the source code location is drivers/hwmon/ina2xx.c, but hwmon is not visible in /sys/bus/i2c/drivers. I found hwmon in /sys/class, but when I entered hwmon0 inside, I couldn't find ina2xx.c. I would like to know where I can find ina2xx.c. 

https://www.nxp.com/docs/en/supporting-information/QORIQ_LS1046A_BSP_V0-4_REV-A.pdf 

odasong_1-1697158757388.png

odasong_3-1697158831517.png

 

Additionally, there is a problem that a total of 3 ina220s are used, but only 1 is captured. Is it correct to put the i2c address in channel@2 of the default node in ina2xx.c as shown in the picture below? Also, it would be nice if you could tell me where to modify the calibration register.

odasong_0-1697158664260.png

 

0 Kudos
Reply
1 Reply

1,606 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please enable the following options in Linux Kernel configuration file and rebuild Linux Kernel. It seems that these options are not enabled by default.

CONFIG_I2C_MPC=y

SENSORS_INA2XX=y

In the dts configuration, reg is I2C address of the device.

ina220@44 {
compatible = "ti,ina220";
reg = <0x44>;
shunt-resistor = <1000>;
};

0 Kudos
Reply