analog accelerometer automotive

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

analog accelerometer automotive

1,750件の閲覧回数
morlinic
Contributor I

I'm interested to know if NXP have this kind of sensors:

AUTOMOTIVE ANALOG ACCELEROMETERS (with package like in attachement - chip inside an automotive package) with this specifications:

  • Range about from 3G to 20G (+/-)
  • Sens 50mV/G
  • Automotive qualification
  • As small as possible

use for active/road noise cancellation 

thanks in advanced

ラベル(1)
0 件の賞賛
返信
1 返信

1,630件の閲覧回数
lisettelozano
NXP Employee
NXP Employee

Hello Cristian,

 

We do not have any active analog accelerometer with automotive qualification; we only have digital accelerometers that are active (and recommended for new designs) like the MMA69xxKQ family.

 

We do have the FXLN83xxQ which is an analog accelerometer but is not automotive qualified. The operating temperature range is between –40 to +105 °C and the accelerometer operating ranges are ±2, ±4, ±8, ±16 g dynamically selectable. The sensitivity depends on the range, you can see the details in the datasheet on page 9 here

 

Best Regards,

Lisette Lozano

0 件の賞賛
返信