analog accelerometer automotive

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

analog accelerometer automotive

1,735 次查看
morlinic
Contributor I

I'm interested to know if NXP have this kind of sensors:

AUTOMOTIVE ANALOG ACCELEROMETERS (with package like in attachement - chip inside an automotive package) with this specifications:

  • Range about from 3G to 20G (+/-)
  • Sens 50mV/G
  • Automotive qualification
  • As small as possible

use for active/road noise cancellation 

thanks in advanced

标签 (1)
0 项奖励
回复
1 回复

1,615 次查看
lisettelozano
NXP Employee
NXP Employee

Hello Cristian,

 

We do not have any active analog accelerometer with automotive qualification; we only have digital accelerometers that are active (and recommended for new designs) like the MMA69xxKQ family.

 

We do have the FXLN83xxQ which is an analog accelerometer but is not automotive qualified. The operating temperature range is between –40 to +105 °C and the accelerometer operating ranges are ±2, ±4, ±8, ±16 g dynamically selectable. The sensitivity depends on the range, you can see the details in the datasheet on page 9 here

 

Best Regards,

Lisette Lozano

0 项奖励
回复