David,
Thanks for replying.
The unit is a shock and tilt alarm for an automotive customer.
It’s working OK in normal mode alarm mode over the full temperature range.
We have a self test/ production end of line test mode where we test all functionality of the hardware and compare normal and test mode accelerometer values.
We are also using this mode during our Product Validation Testing as the temperature chambers all have mechanical noise that affect the sensor readings.
Just as a go , no go test before and after other tests
We think several units have a smaller step than others at the minimum temperature.
I had the test window at +1000 in test mode. Some work OK, others we think are less than this value when you get below -35C.
We will keep investigating
Thanks again for your response.
Regards johnc