Will the MP3V5010DP pressure sensor work at all below 2.7V?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Will the MP3V5010DP pressure sensor work at all below 2.7V?

Jump to solution
570 Views
BillHoyt
Contributor I

The MP3V5010DP pressure sensor is rated to operate from 2.7V to 3.3V, but if we ignore its accuracy, will the sensor still operate (inaccurately) below 2.7V?  I have a prototype that we're designing that could operate down to 2.0V if the pressure sensor could at least function down to there.  The measurements could be very far off in this specific application...

Labels (1)
Tags (1)
0 Kudos
1 Solution
383 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

It is not recommended to use the MP3V5010DP with a power supply below 2.7V since data is not characterized at this voltage, but according to the ratiometric nature excitation range of this sensor, it should work, but the accuracy and linearity data of the datasheet would change (operating the device at a different range may induce additional error).

The output given by the sensor is not specified because there is no characterization data at this voltage.


Have a great day,
Jose Reyes
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
384 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

It is not recommended to use the MP3V5010DP with a power supply below 2.7V since data is not characterized at this voltage, but according to the ratiometric nature excitation range of this sensor, it should work, but the accuracy and linearity data of the datasheet would change (operating the device at a different range may induce additional error).

The output given by the sensor is not specified because there is no characterization data at this voltage.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos