Will a 12V voltage supply kill a MPX5050?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Will a 12V voltage supply kill a MPX5050?

488 Views
garvin
Contributor I

Will a 12V voltage supply kill a MPX5050 pressure sensor? Or, will it only effect the reading of the pressure?

Labels (1)
0 Kudos
Reply
2 Replies

328 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Jia Gao,

The required voltage supply for the sensor should be between 4.75V and 5.25V, powering the integrated sensor at different voltage (12V in this case) than the specified in the datasheet can probably not kill the pressure sensor (I cannot warranty that) but is not recommended because the offset, temperature coefficient of offset (TCO) and temperature coefficient of span (TCS) trim will be invalidated and will affect the sensor accuracy and veracity.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

328 Views
garvin
Contributor I

Thank you, Jose.

0 Kudos
Reply