Which sensor most suitable for my application?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which sensor most suitable for my application?

1,282件の閲覧回数
sarahd
Contributor II

I am currently using MPX5500DP for a simple arduino car counter - it measures the change in pressure of a sealed tube when a car drives over it.

The readings from MPX5500DP are not precise enough however; which sensor would I be able to get a more precise reading in ambient outdoor temperatures?

ラベル(1)
タグ(3)
2 返答(返信)

1,195件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

The MPX5500DP have a pressure measurement range from up to 500kPa, which, from my personal point of view, seems high for your kind of application. For more precision, I would recommend to use a smaller pressure range sensor so you can have higher voltage on the output when the car drives over the sealed tube.

 

You can start testing using the MPX5100DP, which is a very similar sensor to the MP5500DP, but with smaller measurement pressure range (0 to 100kPa).

MPX5100DP datasheet: https://www.nxp.com/docs/en/data-sheet/MPX5100.pdf

Regards,

Jose

NXP Semiconductors

1,195件の閲覧回数
sarahd
Contributor II

Thank you for the quick reply! I'll give that a try.

0 件の賞賛
返信